Dear amateurs of electronics,
I am using a Simultaneous RFID Tag Reader (SEN-14066 M6E Nano, as a shield for the Arduino Uno) with the UHF RFID Antenna (RP-TNC) WRL-14131 in order to read Ultra-Small UHF RFID Tag Rain (KIT-16464).
PCB antenna of M6E Nano reads perfectly Ultra-Small UHF RFID tags (applying Example1 Constant Read sketch). After switching the blobs of solder between PCB and external antennas, UHF RFID Antenna (RP-TNC) doesn’t read tags. I re-enabled the PCB antenna and the reader immediately worked again. I have used two brand new interface cables to define whether cables are defective, it didn’t help. The project is powered through Arduino with a power supply of 9V 1A.
-
Is there something in the hardware set-up that has to be rearranged? Is there anything specific that has to be considered when using UHF RFID Antenna (RP-TNC) WRL-14131?
-
Is there something in software I need to change e.g. in the Example1 Constant Read sketch? Or add a piece of code that e.g. enables the external antenna?
Best regards,
Eduard