Hi, I’m investigating about the possibility to add some RFID readers to my N-Gauge railroad model.
I’ll control the system through a Rocrail instance installed on a Raspberry PI3B, and would like to manage the sensor via WIO.
So the idea is to drive the sensor by a controller like Wemos D2R1 or ESP32 or the new Pico2WH (that’s the best choice as suggested by RocRail developers).
In the RocRail forum a lot of people suggest to use your RFID sensors, in particular the ID-12LA.
Here are the questions:
- How connect the sensor to the controller ? I see that the pins on the sensor are very short, so not possible to use standard dupont cable. Does exist a kind of breakout board that expose pins suitable to be pinned with dupont ?
The pico2WH works at 3.3V, should I use a level shifter between the sensor and the pico ?
I understand the only three cables are needed to connect the sensor (power, GND and the signal one) because it uses the UART protocol.
And finally, do you have suggestions for RFID tags to attach to the wagons and loco , that sould have a very limited size (maximum 10x10mm…)
thanks a lot in advance
Andrea