RGB LED Matrix Panel - 32x64 - Power requirements

Hi there, I have the 64x32 RGB LED Matrix and want to make it portable …

I plan on trying some tests once I make a cable but I do have a question or 2.

The Data Sheet, which is from the Chinese data sheet and they love to use W/m2 for the max power.

最大功耗 (Maximum power) W/ M2 762

now, I’m use to mili amp Hours and figuring things out there. What is the max amp draw for this LED matrix??

I want to hook it up to a External Battery Pack (Thats designed to charge devices) 5V 2.1 A output from a USB cable port.

any thoughts and suggestions?

I’m also looking for a possible Pre-Made USB cable to 4 pin molex connector (to connect to back of the Matrix)

Thanks for any information you can provide.

Eric

Up to 4A, worst case, according to https://learn.sparkfun.com/tutorials/rg … okup-guide.