My Olimex JTAG programmer seems to have given up the ghost–whereas it used to work correctly, now the LED doesn’t even come on when I wire it up to power and ground.
I assume it’s dead.
Two questions:
My Olimex JTAG programmer seems to have given up the ghost–whereas it used to work correctly, now the LED doesn’t even come on when I wire it up to power and ground.
I assume it’s dead.
Two questions:
re question 1.
You can damage you JTAG the usual way you can damage any microcontroller. In AVR-JTAG there is AVR microcontroller if you burn one of the ports or apply reverse voltage on it it will be damaged.
re question 2.
the serial port and parallel port programmers are not more durable, the only difference is that if you do something wrong will destroy your PC RS232 or parallel port and no need to change the programmer but the PC ![]()
and they are not STK500/AVRISP software compatible, you can use PonyProg or AVRdude
Best regards
Tsvetan
Another AVR-JTAG it is, then. ![]()
Thanks for the quick response!