Hi there. I’ve bought 5 ROCKBLOCK 9603N boards from Sparkfun. I’ve got 2 running right, but the third one died after a couple of days of use.
I’m using them connected direct to a Raspberry Pi Zero 2 W like this:
Raspberry 9603N
5V → 8. 5VIn
GND → 10. GND
RX (GPIO15) → 6. TX
TX (GPIO14) → 1. RX
The Raspberry is powered by a LM2596 DC-DC converter module that is connected to a datalogger that has a switchable 12v output that turns the device on every 2 hours. After a couple of days of testing i stopped receiving data. I checked it and the DC-DC converter was off and warm and i tought that it has died, but then i realized the ROCKBLOCK was the problem. Using a multimeter i did a continuity check and found that VCC is shorted to GND. The board seems to be perfect at sight (nothing external shorting it).
I hope you can help me. Thanks in advance. And please tell me if i should be contacting Ground Control instead.