I recently bought a Facet and I’m trying to set it up. I’ve done the following:
- 
Connected it to my home WiFi 
- 
Setup my Thingstream account on the Facet 
- 
Verified the connection on Thingstream’s website and it says “Connected” 
I’ve also tried to set it up with SW Maps (I use an iPhone) but I can’t get it to receive any correction data, the dot never goes green, it’s only showing up in blue.
Here’s a screen dump from the Facet connected with USB:
NTRIP Client connected to ppntrip.services.u-blox.com:2101 at 20:13:19
Rover Accuracy (m): 0.5763, SIV: 29
Rover Accuracy (m): 0.5791, SIV: 31
Batt (93%): Voltage: 4.14V Charging: 2.91%/hr Green
Rover Accuracy (m): 0.5800, SIV: 31
Rover Accuracy (m): 0.5798, SIV: 30
Rover Accuracy (m): 0.5783, SIV: 31
Batt (93%): Voltage: 4.14V Charging: 2.91%/hr Green
Rover Accuracy (m): 0.5765, SIV: 30
Rover Accuracy (m): 0.5754, SIV: 29
Batt (93%): Voltage: 4.14V Charging: 2.91%/hr Green
Rover Accuracy (m): 0.5738, SIV: 30
Rover Accuracy (m): 0.5728, SIV: 29
Batt (93%): Voltage: 4.14V Charging: 2.91%/hr Green
Rover Accuracy (m): 0.5739, SIV: 28
Rover Accuracy (m): 0.5740, SIV: 30
Best regards,
Per