I bought an RTK Torch recently and have been wondering about how it will perform with corrections coming from a local base station vs corrections from PointPerfect. I’m sharing my results so that they might help someone else. I also have questions about the results.
I have a base station based on an RTK Surveyor and TOP106 dual-band GPS antenna. I used PPP and 24 hours of data to determine its location. It’s acting as an NTRIP server and is casting corrections through rtk2go. The base station is about 26 meters from my test location.
I set up the Torch to receive NTRIP corrections from the base station and put it at the test location. Once it connected to my wifi network, it moved quickly into RTK Fix mode. The latitude and longitude error read 11 mm and the “age of differential data” was almost always 2 seconds. I averaged 50 readings and captured this location result: 30.52999699417858,-97.70260421030356.
Then I set up the Torch to receive corrections from PointPerfect and put it at the same test location (+/- 1 mm). It said that the fix type was Single until the first PointPerfect corrections were received and then the fix type changed to DGPS. In about a minute the fix type changed to RTK Float and, about five minutes later, changed to RTK Fix. The latitude and longitude error read 14 mm and the age of differential data varied between 5 seconds and 12 seconds. About a minute after the fix type became RTK Fix, I averaged 50 readings and captured this location result:
30.529997691258917,-97.70260388406844.
According to this set of GPS calculators: https://www.gpsvisualizer.com/calculators, the distance between these location readings is 0.27 inches or 8 cm.
My questions:
- 
Why did it take so long for the PointPerfect corrections to result in a fix type of RTK Fix? Is this related to the long “age of differential data” intervals that I saw? 
- 
For my application, 8 cm is big measurement difference. The PointPerfect website says I should expect an accuracy of 3 to 6 cm. Is the 8 cm difference I measured ‘normal’?