RTK Mosiac X-5 Base for NTRIP Updates to RTK Torch Problems

Any help would still be much appreciated whenever you can get to it!

A few more updates though as I have been messing with it more. I changed the configuration of the rtk mosaic x5 to wifi mode and I was still able to act as an ntrip server base but it also would red line every 10 seconds and the torch still would not connect in SW Maps.

I also tried to reconfigure my torch to connect to wifi and manually enter the ntrip server I wanted to connect to as a client following the directions for using the serial port but I was never able to access the menu, I just kept getting an error which another person is having on this thread Torch serial config.

I was able to connect to the torch on SW Maps for android and connected as an ntrip client but sadly I could only borrow it for a few minutes so I wasn’t able to take enough time for testing to see if I could establish an rtk lock, I could just see that it said I was connected as a client. So now I am thinking maybe the problem is SW Maps on IOS and the new torch are incompatible?

Still looking at all the options for trouble shooting. Thanks for the help!