Hi @allison.roush1 ,
Many apologies. I saw your other post. I suspect your Torch isn’t running the RTK Everywhere Firmware either. That would explain a whole load of badness… Apologies for the hassle. Please upload the 2.1 firmware and you should be able to get corrections.
I have an RTK mosaic-X5 configured the same as yours: Ethernet mode (Ethernet not connected); USB connection to a Windows laptop; “Outgoing Internet Access Over USB” enabled; WiFi \ More Adapter Options \ Sharing \ “Allow other network users to connect through…” (Ethernet 3 in my case). It took me a while to remember the “arp -a” trick to find the new X5 IP address for the Ethernet-over-USB web page, but the Septentrio video was very useful here.
I’m sending corrections from the X5 to RTK2go. I am seeing the same red line “No data sent” issue, every 10 seconds. But, despite that, RTK2go is happy with the connection.
I have an RTK Torch running a fresh install of RTK Everywhere 2.1. Through the serial console, I gave it the WiFi SSID and password. Exited the menu to apply the changes. Re-opened the menu and entered the RTK2go settings using option 1 followed by 7. Exit the menu to apply the settings. The Torch is getting corrections and is RTK Fixed.
I always enter my true email address in option 10 Caster User Name - replacing the default “test” email address.
Please remember that the X5 “Outgoing Internet Access Over USB” defaults to “Off”. You will need to save the change in the “Boot” configuration to enable it at power-on.
Apologies again for the hassle - I hope this helps,
Paul