I have a Portability shield mounted on top of a RTK Postcard. Everything is working fine when plugged into USB. When I try to run off battery, It does not start and has a blank screen. No lights anywhere on either of the boards. The Battery is at 4.0V. Next I tried plugging the usb back in and it boots then immediately “Charge Battery” comes up on screen and nothing else happens. Yes Power switch is on. Lights on RTK board are also on so gps seems to be working. ??
I doubt that your battery is not supplying sufficient current for the whole setup. Even if it is a 4V battery, measure the voltage with a multimeter.
It looks like there should be a small bridge, your unit looks more like a medium bridge to me Hardware Overview - SparkFun Portability Shield Hookup Guide
It might be worth wicking some of that off
Double-check the polarity of the battery vs our connector (labeled), and as suggested above see what voltage the battery is outputting while hooked up
Standalone Battery is sitting at a measured 4.0V.
Awesome!
There’s no industry standard, we just make sure all of ours match the other products and the lipos that we sell ![]()