Postcard + Compatibility Shield Does Not Charge LiPo

I have a Postcard, a Compatibility Shield, and the 850 mAH LiPo battery (Lithium Ion Battery - 850mAh - SparkFun Electronics). The battery worked great to power the system. However, the battery does not charge when it is all powered by the USB connector. Is there something that I must do to enable LiPo charging?

Thanks!

Which position is the power switch up top in?

I have the same setup as described.

My battery charges with the top switch in the off position.

When I connect it to USB, the system turns on.

Do the charging LEDs on the SD portability shield light up?

It’s a long shot but try disconnecting the battery then reconnect and see if that gets it charging.

The “long shot” seems to have worked. I unplugged the battery, plugged it back in, and now the yellow CHG LED is brightly lit and I am happy! ! (Why didn’t I think of that?)

Huzzah!

Thanks!
Len

No problem!
Happy Thanksgiving!