Hi everyone. After all the testing with PPP-HAS, I started having issues with the battery charge.
I have a Postcard and a Portability Shield with a 5000 mAh Lipo battery.
It was working fine and charged very well until two days ago. When I turned off the charging light, it remained at 101% and 4.21 volts, according to the information.
Now it charges very slowly and reaches 4.2 volts, says 58%, and the charging LED turns off.
What could it be?
Poor quality Chinese battery? Fault in the charging system?
I appreciate any ideas.
Regards
Angel
4.2V is the charge termination voltage, so the battery is fully charged. Most PMIC’s need a few cycles before the SOC (% charged) becomes accurate. The PMIC doesn’t know that you’ve installed a 5Ah li-po.
I can’t promise this is what’s happening for you, but it’s not uncommon for PMICs.
If you have a USB power meter, check if charging current actually drops to near zero when LED goes off. If it cuts early (e.g., still plenty of current flowing at ~4.1 V), then the charging circuit might be faulty.
I don’t have a formal method to change the fuel cell profile. Personally, I would just use it knowing that you’ll get many hours of run time because the battery is full, and generally ignore the reported level knowing that it’s artificially low.
Hi everyone.
Update on the situation.
I charged the battery several times, and it still showed 4.2 volts and 58%.
And the yellow charging LED kept going off.
The battery life was still very good, lasting almost a full day.
So I left it on until it shut off due to low battery and charged it again.
It took a long time to charge the 5000 mAh battery, but it returned to the correct values: 4.2 volts and 100%.
We’ll see if it stays that way.
Regards
Angel