I have the RTK Surveyor set up in base mode, and have it connected via telemetry radio to a QGroundControl instance, but I am not able to see RTCM data coming through. When I have it turned on, the base light blinks but never turns into a solid red light. No data is sent through the Radio, and nothing happens. When I directly plug the surveyor through usb to my computer running QGroundControl, it says that there is RTCM data. I don’t know why the surveyor is not sending any RTCM data over the radio.
While we don’t have any experience with QGroundControl, it sounds like there is an issue between the RTK and the serial radio(s) (because it is working when directly hooked up to PC) - can you perhaps try verifying that you can get the RTK and radio to work properly using our suggested methods here https://learn.sparkfun.com/tutorials/sp … 1615791300 and then attempting to implement QGroundControl after ensuring the module is fully functional? It’ll take a bit to complete, but it should help us eliminate some potential issues
Also try swapping the data ports (there are 2) and see if that changes anything ![]()