I don’t know where to post this. I purchased a RTK Surveyor and a Holybro Telemetry unit from sparkfun, expecting to connect the two with the cable assembly from the telemetry package. Holybro changed the number of positions in there connector from 4 to 6. The RTK Surveyor still has a 4 position sensor. Should I make a new cable assembly with one end four position and one end 6? If I do this which pins do I leave out and where do I get the new connector. Should I modify the board of the RTK Unit with a 6 pin connector mounted to the circuit board? Again what signals should I add? Is Sparkfun going to modify the RTK unit to have a 6 pin connector? Did I buy the wrong telemetry kit?
I am really open to your suggestions.
Thank you,
Christopher Howe