Hello,
I have two Sparkfun SAMD21 Pro RF boards and I’m simply trying to get the Hookup Guide point to point example to function. One is running the Samd21_PRF_Client sketch and the other Samd21_PRF_Server. For whatever reason, I canNOT get the server to respond to the client. I have verified using an SDR that the client is sending out its request every 2 seconds which I can see exactly at 921.2 MHz as shown in the sketch. I’ve confirmed both boards are able to transmit by running the client on both boards. Both boards are using the exact same antenna and u.FL connector directly attached to the board.
I’ve also tried running the example sketches from the radiohead library, adjusting them to use the proper pins for the Pro RF board but I still do not get any response from the server.
Anyone else run into this? I feel like I’m going insane. Thanks!