Sparkfun Pro RF board not getting it

I have a couple SparkFun Pro RF boards and I’m just trying to get them working. I’ve loaded the sample server and client but it keeps just stopping at the rf95.init() function and saying Radio Init Failed - Freezing. I’m not sure what I’m doing wrong and I’m hoping someone can help and it’s just something easy and silly that I’m doing wrong. Here’s my code…

#include <SPI.h>

//Radio Head Library:
#include <RH_RF95.h>

// We need to provide the RFM95 module’s chip select and interrupt pins to the
// rf95 instance below.On the SparkFun ProRF those pins are 12 and 6 respectively.
RH_RF95 rf95(12, 6);

int LED = 13; //Status LED on pin 13

int packetCounter = 0; //Counts the number of packets sent
long timeSinceLastPacket = 0; //Tracks the time stamp of last packet received
// The broadcast frequency is set to 921.2, but the SADM21 ProRf operates
// anywhere in the range of 902-928MHz in the Americas.
// Europe operates in the frequencies 863-870, center frequency at
// 868MHz.This works but it is unknown how well the radio configures to this frequency:
//float frequency = 864.1;
float frequency = 915.0;

void setup()
{
pinMode(LED, OUTPUT);

SerialUSB.begin(115200);
// It may be difficult to read serial messages on startup. The following
// line will wait for serial to be ready before continuing. Comment out if not needed.
while(!SerialUSB);
SerialUSB.println(“RFM Server!”);

//Initialize the Radio.
if (rf95.init() == false){
SerialUSB.println(“Radio Init Failed - Freezing”);
while (1);
}
else{
// An LED indicator to let us know radio initialization has completed.
SerialUSB.println(“Receiver up!”);
digitalWrite(LED, HIGH);
delay(500);
digitalWrite(LED, LOW);
delay(500);
}

rf95.setFrequency(frequency);

// The default transmitter power is 13dBm, using PA_BOOST.
// If you are using RFM95/96/97/98 modules which uses the PA_BOOST transmitter pin, then
// you can set transmitter powers from 5 to 23 dBm:
// rf95.setTxPower(14, false);
}

void loop()
{
if (rf95.available()){
// Should be a message for us now
uint8_t buf[RH_RF95_MAX_MESSAGE_LEN];
uint8_t len = sizeof(buf);

if (rf95.recv(buf, &len)){
  digitalWrite(LED, HIGH); //Turn on status LED
  timeSinceLastPacket = millis(); //Timestamp this packet

  SerialUSB.print("Got message: ");
  SerialUSB.print((char*)buf);
  //SerialUSB.print(" RSSI: ");
  //SerialUSB.print(rf95.lastRssi(), DEC);
  SerialUSB.println();

  // Send a reply
  uint8_t toSend[] = "Hello Back!"; 
  rf95.send(toSend, sizeof(toSend));
  rf95.waitPacketSent();
  SerialUSB.println("Sent a reply");
  digitalWrite(LED, LOW); //Turn off status LED

}
else
  SerialUSB.println("Recieve failed");

}
//Turn off status LED if we haven’t received a packet after 1s
if(millis() - timeSinceLastPacket > 1000){
digitalWrite(LED, LOW); //Turn off status LED
timeSinceLastPacket = millis(); //Don’t write LED but every 1s
}
}

Here’s the output I get…

RFM Server!
Radio Init Failed - Freezing

I have the ipex type antennas attached to each board.

I tried soldering the lorawan jumpers on the back but that didn’t help so I unsoldering them again.

Try running the example code as-is, without modifying it: SparkFun SAMD21 Pro RF Hookup Guide - SparkFun Learn

Thx for the reply. I figured it out. I think I had the wrong dev board selected.