SAMD51 - PINS CONFIGURATION

Hello everyone,

I’ve been playing with the SAMD51 CI and it’s variant files. Everything is going really smoothly with the pins programming and when using the Arduino IDE to code. However, I’ve got a question that I could not find the answer and would appreciate if someone could help me understand the problem.

When dealing with the varian.cpp, we have the PinDescription array that basically tells us what is the function assigned to each pin, like the code below.

[...]some code here[...]
{ PORTA, 6, PIO_DIGITAL, PIN_ATTR_PWM_E, No_ADC_Channel, TC1_CH0, TC1_CH0, EXTERNAL_INT_6 },
 { PORTA,  15, PIO_TIMER_ALT, PIN_ATTR_PWM_F, No_ADC_Channel, TCC2_CH1, TC3_CH1, EXTERNAL_INT_2  },

[...]some code here[...]
  { NOT_A_PORT, 0,  PIO_NOT_A_PIN, PIN_ATTR_NONE, No_ADC_Channel, NOT_ON_PWM, NOT_ON_TIMER, EXTERNAL_INT_NONE },

 [...]some code here[...]
{ PORTB,  2, PIO_ANALOG, (PIN_ATTR_ANALOG|PIN_ATTR_PWM_E), ADC_Channel14, TC6_CH0, TC6_CH0, EXTERNAL_INT_2 },
[...]some code here[...]

My questions are, when do I know if I should use PIO_DIGITAL instead of PIO_TIMER_ALT and why not PIO_TIMER?

I know that _ALT, al least for the SERCOM, means the second column (of the two with SERCOM) in the datasheet. However I don’t know a TIMER column.

Also, why would anyone use NOT_A_PORT instead of just leaving without this line?