I’ve bought 12 SEN 10245 sensors (2 for a project, then a further 10 to try to find 2 that work), and I cannot get them to work. I have tried testing the resistance while applying a load and none of them register a resistance change. I have my multimeter connected to the black and white wires and get a reading of around 1950 ohm. When I apply pressure to the sensor there should be a slight change in resistance but so far none of them work.
This video shows the method I am using to test the sensors:
https://www.youtube.com/watch?v=aTn74Fy … nel=Indrek
I also have an HX711 amplifier to connect these sensors to my arduino but cannot get a signal when running the calibration sketch.
Can anyone tell me if I’m doing something wrong? It seems unlikely that all 12 sensors do not work.