Hi
I have some questions regarding the Serial LCD kit:
I use a variety of serial (RS232) devices such as GPS, echosounder and scales which out puts a NMEA string at about 5Hz.
e.g.
$GPRMC,183729,A,3907.356,N,12102.482,W,000.0,360.0,080301,015.5,E*6F
$GPRMB,A,V*71
$GPGGA,183730,3907.356,N,12102.482,W,1,05,1.6,646.4,M,-24.1,M,*75
$GPGSA,A,3,02,07,09,24,26,1.6,1.6,1.0*3D
I would like to know if I connect these using a RS232 shifter (to convert the RS232 to serial TTL) will the NMEA sentence be scrolling on the LCD display.
This would make the Serial LCD a very handy device tester during fault finding.
My second question is what is the 5V power input tolerance? I see some of my devices output about 5.2V. Will the board be able to handle this or do I need to put some voltage regulator in my build?