neeto
                
              
                
              
                  
                  
              1
              
             
            
              Hi Newbie here - be kind,
I’m having trouble getting something sensible to appear on the SerLCD / B&W 2x16 LCD screen.
I’ve got it connect to the serial port on my Vista PC & a 5v power connection from a molex plug.
When I power up the PC I see the splash screen on the LCD and backing light is on.
I’m use the putty program to open a 9600,1,N connection to the LCD on COM1.
The manual says by typing ASCII character’s they should appear on the screen.
I seem to some random characters to appear on the LCD - mostly one for one, but not the characters I typed.
I’ve also tried using LCDSmartie & the SerLCDDerver version 1.1 driver - again I get lots of garbage characters on the LCD.
Any suggestions?
Thanks,
Neeto
             
            
              
              
              
            
            
           
          
            
            
              How did you got it connected to the serial port?
             
            
              
              
              
            
            
           
          
            
              
                neeto
                
              
              
                  
                  
              3
              
             
            
              
b_bogk77:
How did you got it connected to the serial port?
1 wire connection from serial port pin 2 (TX) to RX connector on SerLCD
1 wire connection from serial port pin 5 to GND connector on SerLCD shared with ground on PC power supply.
1 wire connection from 5v power line to 5V connector on SerLCD
Thanks,
Neeto
             
            
              
              
              
            
            
           
          
            
            
              From the LCD’s text information: “TTL serial (do not attach directly to RS232 port).”
TTL means 0v to 5v, RS232 port means -13v to 13v !
You need to use something like this:
http://www.sparkfun.com/commerce/produc … cts_id=316
or this:
http://www.sparkfun.com/commerce/produc … cts_id=449
to interface between the LCD and the RS232 port.
             
            
              
              
              
            
            
           
          
            
              
                neeto
                
              
              
                  
                  
              5
              
             
            
              Ahhh - that would do it - I really should stick to software - this hardware stuff is a whole new mine field 
Thanks,
Neeto