Hello, please tell me about temperature range of work of Serial SD Datalogger, I searched this information but didn’t find.
Thank you for advance.
Hello, please tell me about temperature range of work of Serial SD Datalogger, I searched this information but didn’t find.
Thank you for advance.
If you can provide a link to the SD logger you are referring to, we should be able to assist you further.
Thanks for the clarification. If you take a look at the datasheet for the main IC on the board, the ratings are listed as -40 degC to 80 degC. I would recommend not attempting to operate the datalogger close or at either of these temperatures, as it will decrease the life of the board dramatically, and will likely lead to malfunctions or permanent damage. However, I would use those as your range for the absolute min/max for operation of the board. Keep in mind you may also want to check out the temperature ratings of any components you connect to the Logomatic, as well as the SD card you intend to use. If one of those has a smaller range, you will want to use that as your operating range.
Thank you. I want to use it in negative temparature range, for example (-10 +30), can I do it?
Those values fall within the functionality range for the Logomatic’s ratings, but again, you will want to check the temperature ranges for all of the components you plan on using in your project.