I have one Faucet kit and one Surveyor kit and have used them succesfully as base and rover. However the measured points do not line up with known points which I have recieved from the municipality, the difference is in teh 2-3 m range. Now I would like to set one of the units on a tripod over one of the known points as a base and input the known coordinates into the base unit.
Is this possible on either of the units? If yes, how?