Hi,
I have been observing a voltage drop whenever i connect my ARM-USB_TINY jtag to my development board. The setup is something like this,
-
I connected my developmentboard to a 5 Volt power supply.
-
I checked the voltages at the microcontrollers, it comes out 3.4 which is as expected after the regulator.
-
I switch off the power supply connect the jtag and power the board again.
-
Even now the voltages are exactly as desired.
-
When i finally flash the board, the voltage drops to 4.8 volts.
The voltage drops is hardly 0.2V, but still it should remain stable at 5.0Volts. Not sure if this is a serious problem.
The board is flashed successfully and it works fine. Is this a serious problem. Do you think there might be something wrong with the JTAG or the board.
thanks & regards
Vineet