I could not find any information on whether BacthPCB service supports slotted pads. Is this supported? If so do you just supply a readme file indicating which pads are slotted?
I noticed my drill file just shows two drills at each end of the slot but nothing about routing between them so I assume this has to be described in a readme file.
slammers:
I could not find any information on whether BacthPCB service supports slotted pads. Is this supported? If so do you just supply a readme file indicating which pads are slotted?
Greetings Shawn,
I’ve done one board through BatchPCB with slots. I had my
fingers crossed, as I didn’t request the slots beyond the
way I built the part’s footprint in EAGLE.
I did it by filling the required slot with overlapping drills.
This creates multiple DRC errors in EAGLE. The finished
board had a nicely formed slot with plating on internal
walls. The part is a DC Power Jack that has three blade
contacts for PCB insertion. Ironically, after this effort I
found a version of the same part with round pins…
I’ve seen PCB board houses object to overlapping drills.
I would expect that they would not allow overlapping drills. That would probably cause their bits to break unless it was a large diameter hole. Slots really need to be routed.
I got an email back from BatchPCB saying that slots are not supported.