Again, as Leon_heller stated, find a fab house that can drill that small. Thats crazy small. It’s slightly larger than a human hair. You would have to go into eagle and create a new drill size. I don’t know how to do this but you could find out if you RTFM. Then after you do that, when you create a via select that size from the drop down list. This is all crazy though and its not worth the crazy excessive cost.
Again, as Leon_heller stated, find a fab house that can drill that small. Thats crazy small. It’s slightly larger than a human hair. You would have to go into eagle and create a new drill size. I don’t know how to do this but you could find out if you RTFM. Then after you do that, when you create a via select that size from the drop down list. This is all crazy though and its not worth the crazy excessive cost.
If you can find someone to drill that small, then it is very simple to set the size in Eagle. All you need to is type in the drill size in the box labeled “Drill:” when you are placing the via. It will then remember that drill size.
If you want to change existing vias, click the Spanner on the left, hover over Drill, then click … at the bottom. Type in your required drill size, and then one by one click on each via you want to change.
Basically, it says that the width of the anular ring will be 25% of the drill size. However if this is more than 20mil, it wil be fixed to 20 mil, and if it is less than 10mil, it wil be fixed to 10mil
If you have a 0.2mm hole, that is 8mil. 25% of 8mil is 4mil, which is less than 10, so it uses 10mil. Giving you a total diameter of 10 + 8 + 10 = 28mil smallest size.
If you make the min value smaller, say 5 mil, you would be able to make a 5+8+5=18mil diameter via.