Hey everyone!
I’m designing a board using, primarily, SMD components and had a question about a specific part.
In the SFE library there is a part called RESONATOR-WIDE and I wanted to source the component for this footprint; however, there is no description related to the component, so I’m at a loss when it comes to finding the correct size resonator that would fit this footprint.
Find a suitable resonator and design your own part!
Eh, that is annoying to do though. Ive used sparkfuns SMD resonator package, and I didn’t have toooo much of a problem soldering it.
Make sure the resonator is this size though: 1.3 mm W x 3.2 mm L x 0.9 mm H
or use the one I do: http://www.mouser.com/ProductDetail/Mur … G5almtY%3d
“If you are going for 16 MHz”
I dug in a little because I started wondering. I think the RESONATOR-WIDE-SMD are for this size: 3.4 mm W x 6.7 mm L x 2 mm H
http://www.mouser.com/Search/ProductDet … 00HR50X0RZ
IDK someone correct me if Im wrong. Those are WAY easier to solder.