Solar power

Thanks for your input. However, my question is more about the ALC solar power option:

download/file.php?id=8748

For example, is there any difference compared to the ALC battery power option?

download/file.php?id=8749

I mean, both include a JST 2-pin connector and battery recharging circuit.

For more robust solar power supply, I’m considering picking the banana jack power option in ALC then connecting the PCB to the Sunny Buddy load pins – would that work? ALC says it expects regulated 3.3V input but I’m not sure if the Sunny Buddy output meets that requirement? Its tutorial says “the load should be connected in parallel with the battery” and also “Most panels should work, just make sure they produce an output voltage between 6-20V” – so probably it’s not safe for an ALC PCB?

https://learn.sparkfun.com/tutorials/su … guide-/all