I’m currently using the Sunny Buddy with the 6 watt panel and a 1000 mah battery all from SF. This seems to work well enough, but when charging in full sun, it always stops charging at about 3.9 V (measured on my Particle Argon). I think the measurement is accurate as when the voltage drops below about 3.3V, the unit cuts out waiting for a new charge, which seems about right to me. So, the question is, do I have to do something else to the buddy to let it charge to the max battery capacity? I think that should be ~4.2V, correct?
Thanks.