Hi,
I’m having some issues with a sunny buddy board that I’m looking for some help with. The short version is that I can’t seem to get the board to charge my LiPo consistently. Occasionally the board will charge for 5 - 25 minutes or so before stopping, but the vast majority of the time it refuses to charge.
The parts I’m using:
-
Sunny Buddy PRT-12885
-
2Ah LiPo battery RPT-13855
-
LiPo Fuel Gauge TOL-10617
-
9W 6V solar panel PRT-13784 (this was not purchased from SFE, but I’m using this exact panel)
All of that is connected to an Artemis Redboard so that I can read the LiPo fuel gauge and also read the state of the charge and fault pins on the sunny buddy. (The Artemis RB itself is not currently being powered by the battery.)
I’ve adjusted the voltage at the SET pin on the sunny buddy to be 2.85V with the panel and no battery or load connected. I have not altered the default charge rate.
Symptoms:
When I connect the solar panel to the sunny buddy sometimes (very infrequently) it will begin charging (I can see the charge pin go low, and the voltage reported by the fuel gauge goes up). This will continue for anywhere between 5-25 or so minutes and then charging will stop (again verified with the charge pin and fuel gauge voltage). Throughout this the fault pin never goes low, so it doesn’t seem to be indicating any fault. At this stage there seems to be nothing I can do to get it charging again. I’ve gone so far as to remove all wiring, disconnect the battery, etc., but the behavior doesn’t change. Nothing seems to trigger it to go into charging. This is in full Colorado afternoon sun. The state of charge of the LiPo also seems to have no impact. I get the same results whether the battery is 65% SOC or 2%.
And I want to emphasize that it only starts charging every once and a while. I spent hours with this yesterday and was only able to get it to start charging 3 times after dozens of disconnect and reconnect iterations. It seems to be very random.
Troubleshooting steps I’ve done:
-
Verified the panel is outputting 7.15V in full sun with nothing connected to it
-
Verified the battery has no problems being charged with a different charger (used the SF adjustable charger PRT-14380)
-
Have connected various standard 6-7.5V wall chargers in place of the solar panel and get the same results: charging begins very infrequently and doesn’t last more than ~25 minutes at most when it does start
-
Have disconnected all other items so that only the solar panel and battery were connected to the sunny buddy and left it to charge in full sun for over an hour and noticed no increase in battery voltage
-
Verified I’m always plugging the solar panel into the barrel jack on the sunny buddy and not the artemis

I’m not quite sure what I should check next… Any ideas?
Thanks!
Chris