Solder pad on top

I’m just getting started with Eagle and working on my first board. If the Pads layer is on the bottom of the board, how do a create a header that is installed on the bottom of the board with solder pads on the top like SFE’s breadboard supply? Thanks.

Greetings Rick,

RC:
If the Pads layer is on the bottom of the board, how do a create a header that is installed on the bottom of the board with solder pads on the top like SFE’s breadboard supply?

That's a wrong assumption, the Pads layer is independent

of any other layer. Objects (pads) on layer 17 are printed

in copper on all external layers, and with smaller diameter

on internal layers (i.e. more than two layer boards).

To learn more run the DRC (in the board editor) and select

the “Restring” tab. There is a pictorial sectional view of a

PTH (Plated Through Hole), from which you can see the

EAGLE nomenclature.

For a newbie a lot of this jargon will be as clear as mud.

Stick with it, when you have one board back from the

PCB house it will start to make sense.

Comments Welcome!

So if the top and bottom settings for Pads on the Restring tab of the DRC are the same, I’ll get a solder pad on both the top and bottom of a two layer board. Is that correct? My layers setup is the default (1*16).

RC:
how do a create a header that is installed on the bottom of the board with solder pads on the top like SFE’s breadboard supply? Thanks.

If you use the mirror tool (the icon is a rectangle with a dotted line across the middle, and it’s immediately below the move tool (at least it is in version 4.15)), you can move the header from one side of the board to the other.

Greetings Rick,

RC:
So if the top and bottom settings for Pads on the Restring tab of the DRC are the same, I’ll get a solder pad on both the top and bottom of a two layer board. Is that correct?

Yes.

If you are asking about flipping a polarized component to

the “solder” side from the “component” side (in effect

making a two sided PCB with parts on both sides, you

will need _to mirror _the parts from the component side.

(As noted by Lou in another post).

In all PCB CAD work the final PCB is viewed from above,

and both the components and PCB core are transparent.

For example, any wording on the “solder” side will be

mirrored when viewed.

A good way to grasp these concepts is to throw a few

familiar parts on a test PCB design, and run the CAM

job to create Gerber output files.

These may be viewed independently of EAGLE using a

(freware or shareware) third party Gerber viewer. The

Gerbers are the master phototools that are printed on

to the copper at the board house. (If you print them to

paper you can make a model of your PCB before

committing to production - a useful way to catch

placement errors).

Comments Welcome!