Well my boards showed up today and i have some more questions (sorry i am so new at this, first arduino type board experience).
on the 16 holes for the triggers, do i need to just put 1 trigger wire for each switch on the outside edge of the board and attach my other side of my switches to ground? (for example i have door switches in my car - 1 wire goes to ground while the other goes to my current sound module (which the wavTrigger will replace)
if this is the case can i buy an 8 single pin terminal block with screws to solder into this outside row of holes?
something like this https://www.adafruit.com/product/2141
on the ftdi basic board i cant tell if the black connector on the bottom is make or female so if female do i need to add right angle pins to the wav trigger ? And if this is the case can i leave this plugged in and just power the wav trigger with 5 volts or would i be better to use the barrel jack and only connect the ftdi board when flashing/programming?
I asked about power before on another post and sounds like i need to buy something to lower the power from 12v in a car. Would 5v , 6v , 9v be recommended? i have read various things. I will NOT be using the onboard amp and will instead use the jack to feed a pair of rca’s to a small amp
Thanks