Hi. I’m new to electronics and would like to know if I can wire the potentiometers of the spark ounk so as to mount them into a surface apart from the board… Like can I solder them to wires, mount the potentiometers, have about 6 inches of wire running to the board and then solder those ends to the board?
Can I also do this for the power button and the photocells? I guess what I’m asking is: can I set up the controls so that they can be mounted in different spots on a surface rather than have all of the controls mounted to the pcb? Thanks in advance!
Jay