Sparkfun GPS 17285 Suddenly Drops Satellites In View

I am using the Sparkfun_Bblox_Arduino_Library.h with a NEO-M9N SMA GNSS reader
Without change or notice the number of satellites in view is now being reported as zero.
What happened?

Hi @fredstout3 ,

Try putting the antenna outside, with a clear view of the sky. Also check the SMA connector is correctly inserted and finger-tight.

If you need more help with this, please tell us which microcontroller board, code example and antenna you are using.

Best wishes,
Paul

Hi Paul,
I did all of the above. This was not a brief suspension of satellites-in-view but it lasted for hours. No change in hardware or software . The next day, satellites-in-view returned and has been working since then. The position of the antenna has not changed. So, I have no explanation but considering how well the hardware and software has worked, I can only assume that the fault is mine.
Thank you for contacting me.
Fred Stout

Blockquote
This was not a brief suspension of satellites-in-view but it lasted for hours.

Does it happen regularly? Maybe someone nearby has a GPS jammer running?

No. It only happened one time. All the other GNSS data appeared to be present and looked correct.

Hi Fred,

Jamming or strong interference would be my guess too.

Or did this happen during / after heavy rain? Some of our TOP106 antennas have suffered from water ingress - from a poor weld between the two halves of the case. If the antenna itself has a connector, has the cable connection been waterproofed?

Or an intermittent contact or dry solder joint? Maybe try flexing the cable and the SMA connector - gently - and see if it reoccurs?

I hope this helps.

Best wishes,
Paul

Hi Paul,
The antenna has never been outside the house. A loose connection may well be the culprit here. However, we are preparing to return home to Phoenix following a three week trip to North Carolina. May I ask for a few days delay so I can get home and try some of your ideas out?

I should state that, with the new hardware, the satellites-in-view has dramatically increased. I understand the line-of-sight requirement for the antenna and mine sits on the window sill. I regularly see 20 or so satellites when my original system would get 6 or 7.
Just say’n. I will try out the system when we return home.
Thanks again for your interest and support.
Fred Stout

Hi Fred,

We recommend placing the antenna outside as window glass regularly has a thin metal coating on it. It helps keep the heat out / in, but also does a great job of blocking GNSS signals…

Just reach out again if you need more help. The best place is the GPS/GNSS Forum:

All the best,
Paul