Sparkfun IoT Brushless Motor Driver - not working - ESP32 reset loop

Hi,

I hope this is the right place for the above board.

I followed the hookup guide and programed the board successfully.

However, the board gets into reset loop throwing the reset boot message to the terminal every second, the motor is not running and has no resistance when trying to turn it manually.

I tried another USB cable, another USB 3.0 port and also connecting directly from wall charger but got the same behavior (for the charger there is an on-board LED blinking every second that indicated the reboot loop).

I did try Arduino IDE 1.8.19 and also the latest Arduino IDE 2.21.

I tried the ESP32 DEV board and also the ESP32 Thing Plus C board.

Then I programmed a simple sketch to print a running counter to the terminal and it worked just find.

Any thoughts what could be wrong?

Thank you.

Is the physical reset or boot switch stuck by chance? Have you attempted to upload the default sketch? https://docs.sparkfun.com/SparkFun_IoT_ … e-factory/

If neither of those get it going it’s likely defective; was it purchased from us? If so head over to www.sparkfun.com/returns (contact vendor if purchased elsewhere) and we’ll get ya squared away

Thank you very much for your answer.

I tried the default sketch and it worked. Thank you.

I compared it with the sketch that I had and there is a difference in the pinout. I didn’t even think to check it.

Thank you again. Very much appreciated.

I’m seeing the same problem now while compiling a sketch even if using the default sketch. It’s likely that something is broken by the latest ESP32 platform or Simple FOC library. Can your team verify this? If so, can we get instructions for how to use an older IDE and library versions?

I just verified that the reset is caused by the BLDCMotor init. Not sure why since debugging doesn’t work for this device using OpenOCD.

Hello @TS-Russell , I could really use some support with this. I foolishly designed a whole project around your BLDC devkit before realizing that the SDK was broken. The default firmware worked when I first got the product. It’s only when rebuilding it using the latest Arduino and ESP toolchains that the driver reset occurs.

I’d recommend wiping the arduino folders (here’s a thread with instructions How can I uninstall and purge all remnants of an Arduino IDE install? - #3 by jonman - IDE 2.x - Arduino Forum) and re-install after with the older (functional) lubraries/packages

Can sparkfun list the library versions that are supported?

I don’t have one to test/backbuild with, but that board came out in March of 2023; I’d head to the respective sites and grab the libraries from then and you should be all set

Yeah, that did it. I used platform IO to load the Simple FOC version 2.2.3. Platform IO’s ESP32 platform is also older than the one that comes from Arduino. You might want to let your customers know that they can’t use the Arduino IDE with this product anymore.

So calling BLDCMotor.init() causes a reset of the ESP32? If so, would probably be worth submitting an issue in the Simple FOC repo. IMO it’s a bit extreme to say the Arduino IDE can’t be used with this product, sounds like it’s just a bug in the library.

Although given the popularity of the ESP32 and the Simple FOC library, I would be surprised if a true bug exists with calling BLDCMotor.init() on ESP32 that causes a reset. Maybe Simple FOC had a breaking API change that we need to update our example with?

I found there are several bugs upsteam in the Simple FOC library and the latest ESP32 platform. It may take some time for all of these bugs to get fixed and released. As of now this product cannot be used with the Arduino IDE without knowing the magic combination of older versions of each to install.

I found a combination where there was only one bug in the Simple FoC that I manually fixed in my local install. Unfortunately I cannot get this product to work reliably. I suspect that the 3.3v power supply is too low for it to work if there is any kind of load on the motor at all.

Is there a way I could hack this to provide a higher voltage to the motor driver?

I unmounted everything from the motor and tried again. The results were more promising but still inconsistent. For example, the motor will run for some time using velocity FOC then simply stop. The overprotection doesn’t come on, the software is still executing, but the motor isn’t being driven at all. At other times the motor can’t seem to overcome it’s own resistance and need a little push to get going. It’s feeling like something is defective here if, indeed, others have actually gotten this to work before.

Was it purchased from us? If so head over to Returns (contact vendor if purchased elsewhere) and we’ll get ya squared away

Hi. I wasted a bunch of time on the same issue. After a bunch of work, I determined that “esp32” 2.0.17 (in the Boards Manager. Not “Arduino ESP32 Boards” btw) and SimpleFOC 2.3.1 and SimpleFOCDrivers 1.0.8 (in Manage Libraries) is a valid combination that allows the Sparkfun IoT_MotorDriver.ino sketch to compile and run correctly. Might be worth putting that on the product page?

Also, maybe you’ll never update this board, but it would be pretty trivial to include a jumper to make supplying the driver with higher voltages easier (why is the motor run at 3.3v anyway? Not sure what the thinking there was) and I agree, the PCB looks like it’s designed to break apart, but there are no pads on either side of the break to facilitate this. Neither would be complicated changes.

@scottdarch @michaelrcolton Could you please share the code you’re using? I’d like to try replicating the problem on my end to better understand it and the best path forward.

Thanks!

The problem manifests with the sample code from Sparkfun. The problem seems to be that, I think, both the Arduino ESP32 and SimpleFOC have breaking changes since this board was designed. That’s going to happen, but since there was no documentation about what the code was written to use, anyone using newer versions of those isn’t able to compile it. But with the two versions in my post above it works. To replicate the problem just update your Arduino ESP32 and SimpleFOC to the current versions and try to compile.

(If you are looking for constructive feedback, here’s another: It would have been lovely if the hall sensor on the board was one of the ones that SimpleFOC supports by default, and it would have pretty nice if the sample code used it, rather than FOC in open-loop mode. I bought it expecting all the onboard features to sorta work out of the box, but getting the onboard hall sensor to work with SimpleFOC is proving a little tricky.)

To replicate the problem just update your Arduino ESP32 and SimpleFOC to the current versions and try to compile.

Compile what code? A specific example would be very helpful!

I believe they are referring to Example - Factory Reset - Hookup Guide - SparkFun IoT Brushless Motor Driver

Sorry, I think you may have misunderstood. I’m saying the code from SparkFun that is linked to on the product page:
https://docs.sparkfun.com/SparkFun_IoT_Brushless_Motor_Driver/assets/arduino_examples/IoT_MotorDriver/IoT_MotorDriver.ino