I just got two SparkFun IoT Brushless Motor Driver kits, and neither will connect to my Windows 11 PC.
Regardless of if I have the correct drivers installed, when I plug in the USB, I expect Windows to make that “Bah-dah” sound to indicate it detected new hardware. It does not make that sound.
The “PWR” and the “MPWR” lights both turn on. The “STDY” light turns on. After a few minutes I feel the motor start to heat up. There’s definitely power going to the board. The fact that it heats up is interesting considering that means the motor is getting current when I haven’t programmed anything yet. It also is “locked” into position when power is applied.
There is nothing new under Device Manager/Other Devices. There is nothing new under Device Manager/Ports.
I do have a CP210 ESP32 device that I am able to connect using the same USB port and same USB cable. I can also use the same USB port and cable with my phone and am able to browse its file system. And, of course, in both cases windows says “Bah-dah” indicating something new was connected.
I found nothing in the Event Viewer.
I’d say I’m 100% it’s defective hardware except that I got two and they both have the problem.