Thank you for linking specific example code!
I gave this a test today, and was able to replicate the crashing behavior. I then discovered there’s a new version of Simple FOC and the ESP32 core, both have come out in the last week. Updating those fixed the problem for me. For reference, these are the versions that work for me with that example code:
Simple FOC v2.3.5
esp32 v3.3.0
Skimming through the release notes, looks like Simple FOC recently added support for the esp32 core v3.3 (ESP-IDF v5.x) via this pull request, and more recently fixed an ESP32 bug in this pull request. So, sounds like Simple FOC just hadn’t caught up to the latest ESP32 core, but seems like it should be all good now. If you have any issues with this again, I would strongly recommend opening an issue in the Simple FOC repository, because they will be able to provide better guidance faster than we can.
Hope this helps!
Hi @SparkFro, Im not sure if the latest updates somehow changed something, but while I dont get the reset loop or crashing, the motor doesnt move at all. This is with ESP32 3.3.7 and SimpleFOC 2.4.0.
If I press the buttons, sometimes they will ‘double’ press on the monitor. I dont double press them, but the serial monitor w/ the factory implemented code will show “Changing directions” “Changing directions” or “Starting motor” “Stopping motor”. If you press the buttons a few times, it will crash and reboot the system saying “Guru Meditation Error: Core 1 panic’ed (LoadProhibited). Exception was unhandled.” and tell me “Backtrace: 0x40083c79:0x3ffbfd1c |<-CORRUPTED”.
There are also some issues with the documentation. Firstly, ‘ESP32 Arduino’ does not contain any boards outside of some arduino nano. ESP32 contains the Sparkfun boards. See Installation & Setup - Hookup Guide - SparkFun IoT Brushless Motor Driver