SparkFun Micro OLED Breakout in I2C mode jumper BS1

When using the SparkFun Micro OLED Breakout board in I2C mode, I know I need to set jumper BS1 to 1. In the picture on page 7 of the hookup guide, it looks like all 3 pads (0, center & 1) are all soldered together. Is this correct or do I need to remove the solder bridge between center and 0, and then bridge center and 1? If I short all 3 as in the picture, it looks like I’d be shorting GND to VCC I figure I’d ask before frying something. Thanks.

I agree that it’s kinda confusing. Looking at the schematic, I would say that only the center and ‘1’ should be bridged. Need to remove the bridge from center to ‘0’.