Spectrum shield works with phone mic but not music.

Hi

If I use a smartphone as a mic connected with a mini jack and speak into it the spectrum shield outputs as expected. However, using exactly the same connection, if I play music on the phone the spectrum shield doesn’t react.

Any ideas what I’m doing wrong would be appreciated.

Hi Lisa.

If it works on one, it should work on the other. Couple of things to try:

  • - Make sure your music is actually coming out of the headphone jack and not going to another audio output like Bluetooth or the earpiece on your phone.
  • - Try turning the volume up. If it's too low, the shield can't "hear" it.
  • Thanks for that - the volume was up but the very clever tech at college worked out that the phone was only sending out on Frequency 2! It is working fine now.