Hi
Sparkfun is selling SI4735 AM/FM tuner chip. I kindly ask you to to offer those chips with “SSB firmware”. Silicon Labs have confirmed, it is available, and this chip seems to work well as SSB receiver, on its own class. (Example: http://swling.com/blog/2014/12/a-review … -portable/ )
I also would like to see this “SSB-chip” also on shield and breakoutboard.
This chip have great advantages: It has automatic (and manual!) antenna tuning capasitor, several channel filters, low (real low!) power consumption, s/n meter, kind of squelch, and a lot more, it is awesome for radio amateurs and other persons active on radio.
I have been using discontinued SI4735 tuner shield, and is its surprising receiver. It can be tuned up to 10 meter amateur band (over 28 Mhz) and it can be used for SSB-receiving with external local oscillator. I have received SSB-speech,weatherfax images, Thor-transmissions and CW with it. Image supression is a problem with this kind of setup. But with SSB-firmware it could be a good SSB-receiver.
RasPi can be used as a barebone RF-transmitter. With this chip it could be used as a ham-transceiver. With Arduino style boards, AD9850 DDS-board (cost around 10 dollars) can be used for transmitting and with SI4735 “SSB-chip” it makes real ham-transceiver.
I guess Sparkfun only have to order these chips with SSB-firmware…so please please… ![]()