Hello forum,
From the V13 hookup guide:
Charge current = 1/(R1*Rsen)
Also given, Rsen = 1ohm will give 550mA charging current.
This implies=> R1 = 1/0.55 ohm
So to get 2A charging current(max limit of IC) => R1*Rsen = 1/2
So Rsen = 1/(2R1)=1/(2(1/0.55)) = 0.275 ohm = 275mOhm
Is this doable.?
Also, can the inductor withstand this output.? Because a saturation issue is found mentioned in some articles.
Thanks,
mahesh
Hi mahesh,
Unfortunately, you will not be able to set the charge current for the Sunny Buddy to 2A without switching inductors. The inductor on the Sunny Buddy has a max spec of 1.05A and the inductor will probably start to saturate above ~850mA. The engineer who designed this board replied to a similar question in the [comments on the product page.](https://www.sparkfun.com/products/12885#comment-55117659ce395f5d4d8b4567)
Hi TS-Mark,
So how efficiently someone can charge a 6000mAh battery using a 6W/8.8V panel connected to sunnybuddy.?
850mA would be small enough for it. Is there a recommended fix (or change inductor) here.?
Thanks
A short answer is not very efficiently. The peak power output of this [6W Solar Panel is 6V/1025mA in full sun and optimal conditions. Even with the Sunny Buddy configured to output at ~850mA it will most likely take over a day to charge a fully-discharged 6Ah battery since you will most likely not have 7 hours of optimal conditions in a single day. That is also assuming there is no load on the battery discharging it.
You could try adding a custom resistor to the R SEN pads on the Sunny Buddy to adjust the charge current. That is covered in the “Battery Output” section of the [Sunny Buddy Hookup Guide. We cannot help with adding a custom inductor to try and further boost the output of the Sunny Buddy.](Sunny Buddy Solar Charger V13 Hookup Guide - SparkFun Learn)](Solar Panel - 6W - PRT-13783 - SparkFun Electronics)