Sparkfun Community -
Issue as of 29MAY25:
Today, when I was using SW Maps (iOS) and after clicking “connect” to the RTK Facet L-Band Rover, the connection values such as; lat/long, etc. are 0. The connection data (at the bottom) disappears after 1-2 seconds. I’ve been using the same equipment and software for over two years - no issues.
Did anyone else experience similar connection issues after the SW Maps update on iOS v1.2.3 (May 26)?
Troubleshoot so far: deleted SW Maps, re-installed the app, updated L-Band firmware from v4.0 to v4.2., used SW Maps on both my iPhone and iPad running the latest iOS, ran “get keys” - still not connecting.
Thanks in advance!