Using the Surveyor with SW Maps, I’ve tried two methods of getting valid ubx log files. By valid is meant submitting to Emlid Studio or GNSS Converter and not getting an error. Visually inspecting files from the two sources confirm that they are strictly text files (no binary content as ubx files should).
The two methods are 1) checking the “Log to File” when connecting to Bluetooth GNSS and 2) the log files written to the microSD card.
The SparkFun Surveyor ubx files recorded by SW Maps (via BT connection) and the log files recorded to the microSD chip both contain only NMEA text data, no binary records at all. Put differently, all of the ubx files I’ve managed to record do not contain RAWX data.
Hello, SW Maps has a “Log to File” option that will log everything it receives.
Since RAWX and SFRBX messages are a bit bulky, we suggest you to use the USB OTG interface instead of the Bluetooth connection (SW Maps supports both).
original poster rereplied:
Thank You! SW Maps now saves an *.ubx-File. Then I tried to convert the ubx to a RINEX file via RTKCONV ver .2.4.3 b34, but with no success.
I tried “Staff” advice myself using USB OTG, the logged ubx file still are text only NMEA data. I’ve tried connecting as SparkFun RTK, ublox RTK, and ublox; none of them produce log files w/ any binary content.
So far, I’ve found no method to obtain binary-containing ubx files. Am I missing something?