Telit GE 865 + #SD - Socket Dial problem

hello

I am really weak in networks how ever I tried to creat some tcp application by connecting telit gsm module to my local server

when I send this string to the modem it malefunction and I never get connect

AT#SD=1,0,2333,"MY server IP address ",0,0,0 

I also get erorr when I try to send email

but I can open a socket connection in command mode


~~~
AT#SD=1,0,2333,"MY server  IP address ",0,0,1 

Iget OK back from the modem and then I can send data to the server though the internet however I got error after I accept incoming connection from the server 

```
AT#SD=1,0,2333,"server IP ",0,0,1 

OK

SRING: 1
AT#SA = 1,1 

ERROR
```

this are my gprs sittings 

```
AT+CGDCONT=3,"IP","vodafone.com.qa", "0.0.0.0"

OK

+CGQREQ: 1,0,0,0,0,0

AT#sgact=1,1

#SGACT: 10.103.34.205

OK
```

if any one have any Idea please help

Hi,

I use vodafone (on a GM862 and GE864) here in Australia. The following is the sequence that I use to get to a Web Page:-

AT#GPRS=1 //This replies with my IP number I do not even need to specify the apn

AT#SKTD=0,80,“www.theage.com.au” //the 80 is for port 80 the HTML port - replies with connect

GET / HTTP/1.0 //don’t forget cr lf at the end

//needs another cr lf at the end

Then down comes the HTML from the web - it disconnects at the end but I just redo the socket dial - NOT the GPRS = 1

Hope it helps.

john_melbourne:
Hi,

I use vodafone (on a GM862 and GE864) here in Australia. The following is the sequence that I use to get to a Web Page:-

AT#GPRS=1 //This replies with my IP number I do not even need to specify the apn

AT#SKTD=0,80,“www.theage.com.au” //the 80 is for port 80 the HTML port - replies with connect

GET / HTTP/1.0 //don’t forget cr lf at the end

//needs another cr lf at the end

Then down comes the HTML from the web - it disconnects at the end but I just redo the socket dial - NOT the GPRS = 1

Hope it helps.

Thank you Sir I’ll try your sequence

I’ve noticed a similar problem with the 865 QUAD. If I use the newer command set, AT#SGACT=1,1 followed by AT#SD=1,0,80,“some host” the module will hang and give no CONNECT or ERROR. If I use the older commands, AT#GPRS=1 followed by AT#SKTD=0,80,“some host” it connects just fine. If I +++ escape out and then use the multisocket AT#SD version, it works just fine. Seems like the older commands are initializing something that the new commands are not? Has anyone else experienced this?

I found my Ge865 did the same thing, I could not get a CONNECT response even though I could see my Apache server was serving the requested page back.

I found that if I disable flow control with a AT&K=0 then suddenly I see the CONNECT and my html stuff.

I am using vodafone prepaid in Brisbane Aus.

AT+CGDCONT=1,"IP","vfinternet.au",0.0.0.0
AT#USERID=""
AT#PASSW=""
AT#GPRS=1
AT#SKTD=0,80,"google.com"

T

i am having problems sending an email. I used these

AT#ESMTP=“smtp.live.com”

OK

AT#EADDR=“*****@hotmail.com”

OK

AT#EUSER=“*******@hotmail.com”

OK

AT#USERID=“**********”

OK

and then i tried to send the email. but got an error. I do have an active gprs connection.