TF-Luna (ToF) Micro Single-point Ranging LiDAR (Detecting Range: 0.2~8m)

This amazing product specs is :

TF-Luna can detect objects with a minimum edge length of 3.5 cm within a detection distance of 1m;

TF-Luna can detect objects with a minimum edge length of 28 cm within a detection distance of 8m;

Therefore if we use this sensor in a dusty environment like (Cement Silo) could it work well ? as it does not affected by small particles like dust therefore light could not be scattered , I hope my theory is right and if not do you have a laser or infrared sensor can work in dusty environment like cement silos?

Only way to know for sure would be to give it a try. If it does work, the range would probably be lower than normal though.