Hello, I am configuring a remote wireless communication with Arduino board loading a zed-f9p through the UART1 serial port. But the control of U-center hasn’t been possible with the UART1. Does the U-center only allow the connection with USB? But at the moment it looks very hard to attain the wireless communication with the USB connection. Can anybody suggest a way to avoid this difficulty? The use of a serial-to-usb converter may not help since it is also of a usb connection I guess. To say again, my ultimate purpose is to control the U-center through a wireless communication.
Generally u-center is used to set configs or push/pull data…what are you wanting to change live?
Their guide https://content.u-blox.com/sites/default/files/u-center_Userguide_UBX-13005250.pdf makes me think it needs to be something that enumerates as a serial COM port (our guide also touches on this)
You can add a used laptop into the mix to make things easy if you NEED u-center on-the-go
uCenter Classic just needs a COM port instance
The ZED-F9P takes CMOS levels, nor RS232, so you can’t wire in via a DB9 or DB25 serial connection directly.
A Telemetry Radio should work, baud rate matching those of the ZED, and air-rate probably a tad faster so as not to choke