Tiny AVR programmer and pin PB5/RESET (pin 1) of ATtiny85

Using the Tiny AVR programmer, can I program ATtiny85’s pin PB5/RESET as a generic GPIO or ADC input? If I do so, will the programmer be able to reprogram it next time? (I guess it has to be able to apply 12V to this pin.)

Hi, thanks for writing in.

If you change the fuses to allow PB5 to act in a way other than a reset pin you cannot simply reprogram the ATTINY85 via an ISP programmer.

You would have to reset the fuses with a high voltage programmer. Something like another Arduino dev board could work.

Here is a resource to take a look at for further information:

http://www.technoblogy.com/show?LSE

Hope this helps.

Thank you very much!