My Arduino IDE won’t find the Tiny AVR programmer in the “ports”.
Any known issues, or work arounds?
Thanks
My Arduino IDE won’t find the Tiny AVR programmer in the “ports”.
Any known issues, or work arounds?
Thanks
I recall having issues with my Tiny AVR on a PC when hooked up to a USB-3 port; when changing to a USB-2 it worked.
Try unplugging and replugging the Tiny AVR Programmer back into your USB port. Or switch out your USB extension cable for a known good. In some cases, your Tiny AVR Programmer may shows up under the libusb-win32 devices as an Unknown Device #1. If that is the case you should be good to go!
If you are using the programmer with IDE 2.0-rc6 or older, there is a bug in the software that will not allow uploading without a port selected. The Tiny Programmer has no port. The work around is to use “Upload Using Programmer” in the Sketch Menu. I have never had problems with IDE 1,6 up through 1.8.19. But now that IDE 2.0-rc6 allows programming with the Tiny Programmer and programming teensy 4.1, I no longer need to use the IDE 1.8.19! I hope this helps!
Preston