Hello!
This is my first time working with low level hardware. Please forgive my ignorance ![]()
I recently picked up a SparkFun Blues Wireless MicroMod Starter Kit. I’ve been attempting to complete the tutorial on Blues’ website, but haven’t succeeded.
When I plug my USB cable into the main board - no COM port is shown in Device Manager (Windows 10). If I put it into DFU mode by holding boot + tapping reset then I see “STM 32 BOOTLOADER” shown in Universal Seris Bus devices. So, I believe my cable works OK and my computer can see the device, but it does not see it as being able to communicate.
I can upload sketches to it through the Arduino IDE and don’t get any errors, but the code doesn’t seem to run as far as I can tell. Here’s the output I get when I upload some basic example code:
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : STM32 BOOTLOADER
SN : 325037773132
DFU protocol: 1.1
Board : --
Device ID : 0x0413
Device name : STM32F405xx/F407xx/F415xx/F417xx
Flash size : 1 MBytes (default)
Device type : MCU
Revision ID : --
Device CPU : Cortex-M4
Memory Programming ...
Opening and parsing file: sketch_may17b.ino.bin
File : sketch_may17b.ino.bin
Size : 42.30 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
sector 0000 does not exist
sector 0001 does not exist
sector 0002 does not exist
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.206
RUNNING Program ...
Address: : 0x8000000
Start operation achieved successfully
I looked into drivers for it but the latest explicitly shipped drivers were for Win7/Win8. There’s a note in the README that says:
* V1.5.0 - 02/05/2018
=====================
New Features
************
+ Install simplified for better user experience depending on Windows OS,
+ For Windows 10, use Microsoft inbox driver and not this package.
which I think means that it should be plug-and-play in Windows 10.
https://community.st.com/t5/stm32-mcus- … d-p/437577 this person describes a similar issue, but their resolution was soldering?? It’s unclear if that’s my issue and that’s too extreme of a step for me getting my hands dirty.
It’s not clear to me if I’m wildly off base somewhere. I am able to get a COM port when I plug a USB into my Notecarrier Function Board but when I query the state of the function board it’s not updated to reflect the commands that should’ve been sent by the firmware I uploaded to the processor.
For clarity, here’s the code I’m uploading:
#include <Notecard.h>
#define productUID "com.gmail.Meo.DDR:feed_connect"
#define usbSerial Serial
Notecard notecard;
void setup() {
delay(2500);
// put your setup code here, to run once:
usbSerial.begin(115200);
notecard.begin();
notecard.setDebugOutputStream(usbSerial);
J *req = notecard.newRequest("hub.set");
JAddStringToObject(req, "product", productUID);
JAddStringToObject(req, "mode", "continuous");
notecard.sendRequest(req);
}
void loop() {
// put your main code here, to run repeatedly:
}
After I upload this, I tap reset on my main board, wait, and then un {"req":"hub.get"} but I see my mode is still in “periodic” not set to “continuous”
Thanks for your time