TRW-24G Range

Hi!,

Well I finally have something working! I set RF Power to Max (0db)

and my address is set to 8 bits. Since my current range is

30-40 meters a far cry from the specd 280 meters :? Has anyone

actually achieved 100-150 meters 100 % of the time with the TRW-

24G module? If so how was it configured? I’d say in my test works

70% of the time. Below is part of my config settings any suggestions

would be appreciated.

mango4u

/*
    23: 0 Payloads have an 8 bit address
    22: 0
    21: 1
    20: 0
    19: 0
    18: 0
    17: 1 16-Bit CRC
    16: 1 CRC Enabled

    15: 0 One channel receive
    14: 1 ShockBurst Mode
    13: 1 1Mbps Transmission Rate
    12: 0
    11: 1
    10: 1
    9: 1 RF Output Power
    8: 1 RF Output Power

    7: 0 Channel select (channel 2)
    6: 0
    5: 0
    4: 0
    3: 0
    2: 1
    1: 0
    0: 0 Transmit mode
             
*/                

//Clock in address
    rf_address = 0b.1110.0111; //Power-on Default for all units 
    for(i = 0 ; i < 8 ; i++)
    {
        TX_DATA = rf_address.7;
        TX_CLK1 = 1;
        TX_CLK1 = 0;
        
        rf_address <<= 1;
    }

I havn’t tried it but I know you’ll over double your distance by lowering the bitrate to 250kbps since the sensitivity increased by 10 dB’s

Hi,

I have achieved 100-150m with TRF/W-24G with line-of-sight and speed of 250kbps, with packet loss = 0%. But when I put my hand near one transciever, some packets do get lost :x

Without line-of-sight the range is about 30-40m maximum…

What about building RF amplifier? 8)