I am using a Tsunami Wav trigger for an outdoor public art exhibition in display gardens that goes for 6-months, it is solar powered and needs to operate within specific hours. I am trying to get a continuous random playback of a bank of files so that the sounds are always changing, rather than having a static piece which played through on repeat. I had thought to use a simple timer to turn the system on and off but have run into some problems.
I am having two issues:
One is that I can’t seem to work out how to continuously trigger the files to play randomly rather than just once through before stopping?
I have had this set up work before but can’t get it to work this time. I’m using the stereo firmware to randomly trigger a bank of files, but can only seem to get them to trigger once, on startup(invert) or with a shorted trigger(without invert selected).
Is this possible to do this without attaching an Arudino, so that it retriggers automatically?
The second issue is that powering off the system to click before having to manually reset. Is this a power supply issue? should I simply run them separately an only put the timer on the amp, functionally leaving the Tsunami on 24/7
The site is quite far away and I can’t manually restart every day.
Appreciate any advice!